NEWS
 

STMicroelectronics Advances IGBT Switching Performance for Higher Efficiency and Reduced Size in Energy-Saving Ballasts and Converters

Ultra-low turn-off energy boosts efficiency and enables higher operating frequencies

Click for larger image Geneva, May 13,2008 - STMicroelectronics (NYSE: STM), a world leader in power semiconductors, has introduced IGBTs that use innovative and efficient lifetime-control techniques to reduce energy loss during turn off. New devices, including the STGxL6NC60D 600V PowerMESH™ IGBT, allow designers to use robust, low-cost IGBT technology in energy-sensitive circuits such as lighting ballasts operating well above 20kHz, achieving greater overall efficiency than standard-technology MOSFETs.

The improvements in switching performance also allow designers to use IGBTs highly competitive designs with hard-switching topologies as well as with resonant circuits. In addition, the lower turn-off energy allows the device to operate at low junction temperature with a small snubber capacitor, leading to greater benefits including reduced power dissipation, greater reliability and a smaller footprint.

Compared to conventional MOSFETs, ST’s new IGBT technology delivers significantly better performance per die area, to enable a reduced-cost solution. As a further benefit, a co-packaged ultra-fast soft-recovery diode ensures high dV/dt immunity not achievable with other power devices. Applications for this new range of hyper-fast IGBTs include high-frequency lighting ballasts from 70W to 150W, as well as switched-mode power supplies, power-factor controllers and other high-frequency power-switching applications.

The four devices that make up the STGxL6NC60D series provide a choice of power packages, with TO-220, TO-220FP, DPAK and D2PAK options. Prices start at $0.35 for the STGPL6NC60D in the TO-220 package, for orders over five million pieces.

Further information is available at www.st.com/igbt

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2007, the Company's net revenues were $10.0 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2008





Should you require more information, please select the appropriate contact from the "Related Topics" menu.