NEWS
 

STMicroelectronics Introduces Low-Cost Standard-Definition Set-Top Box Decoder Supporting Leading Security Standards and Multiple Codecs

Single-chip decoder for all ‘standard-definition’ markets, shares features and technology roadmap with leading-edge STi7109 ‘high-definition’ architecture

Click for larger image Geneva, December 20,2007 - STMicroelectronics (NYSE: STM), the world’s largest supplier of silicon chips for set-top boxes (STBs)*, today announced a new low-cost STB decoder chip – the STi5202 – intended for standard-definition (SD) terrestrial, cable, satellite and IP (Internet Protocol) TV applications, and for both retail and operator-supplied boxes. It shares the same architecture as ST’s STi7109 single-chip H.264 high-definition (HD) decoder, highly successful in markets worldwide, and it is also software compatible.

The STi5202 integrates an advanced video decoder supporting the H.264/AVC coding standard and MPEG-2, together with a flexible multi-channel audio decoder that handles all broadcast audio standards. For content protection, it includes ST’s fourth-generation security technology, as used in the STi7109, which allows the chip to support Windows Media DRM 10 and the Secure Video Processor (SVP) standards, both protecting content and allowing digital rights to be passed between consumer devices.

Additionally, building on the exceptional performance of the mixed software/hardware decoding engine available on ST’s  STi710x families, the STi5202  also supports Flash video, DivX and videoconferencing standards, as well as the recently established Chinese AVS1-P2 Jizhun Profile 4.0 level (SD) video decoding standard.

Connectivity is provided by on-chip Ethernet and USB 2.0 Hi-Speed interfaces, enabling the decoder to play a key role as a thin client in a home network environment . In addition, optional HDMI (High-Definition Multimedia Interface) can provide SD video for HD displays. A programmable transport stream interface (PTI) manages inputs from satellite, cable and terrestrial tuners.

Embedded in the STi5202 is a powerful 266MHz ST40 CPU core, which is supported by industry-standard operating systems such as Linux and Microsoft Windows CE. ST provides a suite of robust, integrated STAPI software drivers, plus a comprehensive set of hardware and software tools to enable rapid product development. A software evaluation platform and reference design is also available, with full schematics, and with source code for STAPI-based reference software that is compatible with the STi7109.

“We are able to offer our customers this optimized SD solution that will help them to address all segments of the advanced codec market whilst  not compromising on security features or on the powerful multi-processor architecture  ” said Stefano Groppetti, General Manager of the Cable and IP Operators Business Unit within ST’s Home Video Division. “STi5202 shares software with the STi7109 and allows our customers to reduce the cost and improve the time to market when developing mixed SD/HD products .”

The STi5202 is in volume production now, and is available in a 27 x 27mm BGA package, with the same security options as in the STi7109. Pricing for the STi5202 is available on request to STB OEMs.

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2006, the Company's net revenues were $9.85 billion and net earnings were $782 million. Further information on ST can be found at www.st.com.
Information last updated Jan 2007




* ‘MPEG Video ICs: H.264 in the Limelight’ published by InStat. June 2007


Should you require more information, please select the appropriate contact from the "Related Topics" menu.