![]() | ||
|
| ||
STMicroelectronics Introduces Unrivaled High-Performance 64-Mbit Serial Flash for Code-Storage Applications | ||
Geneva,
December 21, 2004 - STMicroelectronics (NYSE: STM) today announced
the availability of a 64-Mbit Serial Flash memory for code storage. This
new device is the world's fastest 64-Mbit serial-interface Flash memory
and has an enhanced data transfer clock speed of 50MHz and read throughput
of 50-Mbit/second. The simple four-line serial SPI (Serial Peripheral
Interface) interface greatly simplifies system design, reduces pin-count,
and offers reduced power consumption via a deep power-down mode that draws
only 1-microamp of current.The M25P64 is the latest and largest density within ST's M25P family and is ideal for code storage in a wide range of applications, such as all-in-one printers, PC motherboards, set-top boxes, CD and DVD players, digital TV, digital cameras, graphic cards, and flat-panel displays. The M25P64 products come in the industry's smallest standard package for comparable products. The 64-Mbit device is offered in a MLP8 package (dimensions of 6x8mm), as well as in a S016 packag,e and uses ST's ECOPACK Pb-free technology for RoHS-compliance (the EU's Restriction on Use of Hazardous Substances Directive). These devices are specified for the -40 to +85 degree C operating temperature range. Built using a high-quality CMOS process, the Serial Flash Memory family offers minimum data retention of 20 years and guarantees 100,000 Erase/Program cycles per Sector, including both Bulk Erase and Sector Erase instructions. The JEDEC standard 16-bit electronic signature allows easy device identification. Samples are available now and volume production is planned for the first quarter of 2005. Pricing is US$6.2 in volume quantities. With densities ranging from 512 kbit to 64 Mbit, ST's Serial Flash family delivers reliable solutions to store embedded program code in low-pin-count and small-footprint packages. Further information on ST's Serial Flash range, including VHDL and Verilog models, is available at www.st.com/serialflash. Programming support for the family is also widely available. About STMicroelectronics STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2003, the Company's net revenues were $7.24 billion and net earnings were $253 million. Further information on ST can be found at www.st.com. |
| ||||||||||||||||||
|