![]() | ||
|
| ||
STMicroelectronics Extends its Serial Flash Family for Data and Parameter Storage with 1-Mbit and 2-Mbit densities | ||
Geneva,
October 22, 2004 - STMicroelectronics (NYSE: STM) has today introduced
two new devices for data and parameter storage within its family of high-speed,
low-voltage, serial Flash memories. The new M45PE10
and M45PE20 will be
used in applications involving a large amount of rapidly changing parameter
data, such as digital answering machines, pagers, video game systems and
electronic toys. These 1-Mbit
and 2-Mbit devices
maintain continuity with the serial EEPROM portfolio and complement ST's
extensive range of M25P serial Flash devices for code storage.The M45PE family offers fine granularity that allows fast-changing data to be stored with minimum system overhead. Each page of 256 bytes can be individually erased and programmed. Furthermore, a Write instruction offers the possibility of updating between 1 and 256 bytes of data. A 256-byte page can be written in 11ms, programmed in 1.2ms and erased in 10ms. In addition, the architecture of the M45PE is optimized to reduce the application software to a minimum, without the need for specific data storage management software in Flash. The devices are accessed through a standard SPI bus with an enhanced clock speed of 25MHz for data transfer. They operate on a 2.7V to 3.6V supply voltage, and, to reduce power consumption, feature a deep power-down mode that draws only 1-microamp. The serial bus architecture dramatically lowers the pin count of the bus master, so lowering overall system costs. Use of these new memories will also extend to portable scanners, fax machines, digital cameras, cellular phones, voice memo recorders, PDAs, MP3 players/recorders, and GPS and measurement systems. The M45PE10 and M45PE20 are available in the S08 Narrow (150mils) package, and in the very thin 8-pin MLP (Micro Leadframe Package) which achieves an SO8 footprint and uses ST's ECOPACK Pb-free technology for RoHS-compliance (the EU's Restriction on Use of Hazardous Substances Directive). These devices are specified for the -40 to +85 degrees C operating temperature range. Minimum data retention is 20 years and write endurance is 100,000 cycles. ST's Serial Flash M45PE family now offers 1-Mbit, 2-Mbit, 4-Mbit, and 8-Mbit products. A 16-Mbit device is planned for 2005. Samples of the new devices are available now and volume production is ramping-up. US pricing, for volume quantities, is $1.10 for M45PE10 and $1.25 for the M45PE20. Further information on the M45PE family is available at www.st.com/serialflash. About STMicroelectronics STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2003, the Company's net revenues were $7.24 billion and net earnings were $253 million. Further information on ST can be found at www.st.com. |
| ||||||||||||||||||
|