Section
Author's Guide | Reviewer's Guide

ST Journal of Research
Index (Vol. 3, No. 2)

Multimedia Streaming Technologies
 

Consumer and PC technologies are rapidly converging, creating a new and global market, where once independent devices are now fused together to provide exciting new services, applications and products for the end users. Arguably, one of the most striking examples of such convergence is multimedia streaming, either in the home or in mobile scenarios. This new application integrates technologies once found only on consumer systems (such as multimedia coding/playback, content protection) with others once found only on computer devices (e.g., the Internet Protocol and packet-based communication). (More...)

 
Vol. 3, No. 2, December 2006 - Table of Contents
Art. 1 Rate-distortion-complexity Modeling for Network and Receiver Aware Adaptation by M. van der Schaar, Y. Andreopoulos, UCLA p. 4
Art. 2 STP-Tool: A fully scalable wavelet video coding scheme with homologous inter-scale prediction by Nicola Adami, Michele Brescianini, Riccardo Leonardi, Alberto Signoroni, University of Brescia p. 19
Art. 3 Performance evaluation of transcoding algorithms for H.264 by D. Lefol, D. Bull, N. Canagarajah, University of Bristol p. 36
Art. 4 Performance evaluation of FMO to improve the error resilience of H.264/AVC by Pierpaolo Baccichet, Stanford University, Antonio Chimienti, CNR, Emanuele Quacchio, STMicroelectronics, Enrico Magli, Gabriella Olmo, Politecnico di Torino p. 46
Art. 5 Robust Transmission of Video using Frame-Based Multiple Descriptions by Riccardo Bernardini, Marco Durigon, Roberto Rinaldo, Pamela Zontone, University of Udine p. 61
Art. 6 A 565 Mbps Multi-Rate IP-core Decoder of Structured LDPC Codes Massimo Rovini, Nicola E. L’Insalata, Francesco Rossi, Luca Fanucci, University of Pisa p. 73
Art. 7 Software and Hardware Implementations of Adaptive Motion Estimation for Real-time H.264/AVC Video Coding Daniele Alfonso, STMicroelectronics; Sergio Saponara, Michele Casula, Luca Fanucci, University of Pisa p. 86
Art. 8 A Multi-Level Approach to Direct Process MP3 Codes in Compressed Domain by Andrea Lorenzo Vitali, STMicroelectronics; Goffredo Haus, Giancarlo Vercellesi, Martino Zerbini - Università degli Studi di Milano p. 98
Art. 9 Adaptive Playout Scheduling with Audio Time-Scaling for the Nomadik Multimedia Processor Giulio Urlini, Andrea Lorenzo Vitali, STMicroelectronics; Antonio Servetti, Politecnico di Torino, Juan Carlos De Martin, CNR, Italy p. 111
Art. 10 Parallel Implementation of Dolby-AC3 Audio Decoder on Multi-Processor SMP platform Yogesh Kumar Soni, Amit Gupta, Kaushik Saha, STMicroelectronics p. 121
 

Download PDF file Full Issue (European A4) Size 7MB
  Full Issue (US Letter) Size 8MB